MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • FRDM-KE16Z board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When running the demo, the debug console shows the menu to tell how to set MCU to target power mode.

NOTE: Only input when the demo asks to input, input at other time might make the debug console overflow and get wrong result.

####################  Power Manager Demo ####################

    Core Clock = 48000000Hz
    Power mode: RUN

Select the desired operation

Press  A for enter: RUN      - Normal RUN mode
Press  B for enter: WAIT     - Wait mode
Press  C for enter: STOP     - Stop mode
Press  D for enter: VLPR     - Very Low Power Run mode
Press  E for enter: VLPW     - Very Low Power Wait mode
Press  F for enter: VLPS     - Very Low Power Stop mode

Waiting for power mode select..