Hardware requirements#
Micro USB cable
FRDM-KE15Z board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal
PFlash Example Start
PFlash Information:
Total Program Flash Size: 256 KB, Hex: (0x40000)
Program Flash Sector Size: 2 KB, Hex: (0x800)
Flash is UNSECURE!
Erase a sector of flash
Successfully Erased Sector 0x3f800 -> 0x40000
Program a buffer to a sector of flash
Successfully Programmed and Verified Location 0x3f800 -> 0x3f810
End of PFlash Example