Hardware requirements#
Mini USB cable
FRDM-KE02Z board
Personal Computer
Board settings#
No special is needed.
Prepare the Demo#
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
Uart functional interrupt example
Board receives characters then sends them out
Now please input:
When you input every character, system will echo it by UART and them would be seen on the OpenSDA terminal.