Hardware requirements#
Mini USB cable
Two FRDM-KE02Z boards
Personal Computer
Board settings#
connect 2# & 6# on J2.
Prepare the Demo#
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
KBI Driver Example Start.
The KBI keyboard interrupt has happened!
KBI Driver Example End.