Hardware requirements#
Mini/micro USB cable
FRDM-KE02Z40M board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
Press the SW1 button to trigger IRQ interrupt, the log is show below:
IRQ Driver Example Start.
The IRQ interrupt has happened!
IRQ Driver Example End.