Hardware requirements#
Mini/micro USB cable
FRDM-K32L3A6 board
Personal Computer
Board settings#
This example project uses LPCMP instance 0(M4) or instance 1(M0) to compare the voltage signal input from channel 2(PTC9) with the voltage signal(half of VDDIO) output by LPCMP’s internal DAC and output different result. LED1 will turn ON/OFF corresponding to different result. So the voltage signal input from PTC9 should be changed to observe the dynamical LED state.
Input signal to J2-18
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
The log below shows in the terminal window:
LPCMP polling Example.