Hardware requirements#
Mini/micro USB cable
FRDM-K32L2B board
Personal Computer
Board settings#
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo#
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
These instructions are displayed/shown on the terminal window:
Starting channel No.0 ...
Channel No.0 interrupt is occurred !
Channel No.0 interrupt is occurred !
Channel No.0 interrupt is occurred !
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.