Hardware requirements#
Mini/Micro USB cable
FRDM-K22F board
Personal Computer
Board settings#
No special setting is needed.
Prepare the Demo#
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
VREF example
ADC16_DoAutoCalibration() Done.
ADC Full Range: 4096
Defalut (Factory) trim value is :34
ADC value: 1336
Use trim value: 0
ADC value: 1340
Use trim value: 4
ADC value: 1338
……
Use trim value: 60
ADC value: 1337