MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • FRDM-IMXRT1186 board

  • Personal Computer

Board settings#

J18(1-2)/J17(2-3): ETH2 Function Via J56B. J12(1-2)/J13(2-3): ETH0 Function Via J56A.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

NETC Switch example start.
Wait for PHY link up...

MAC learning.
The frame received from port 0. Dest Address 54:27:8d:00:00:f0 Src Address 54:27:8d:00:00:00. Port 0 bounds to MAC 54:27:8d:00:00:00.
The frame received from port 2. Dest Address 54:27:8d:00:00:f0 Src Address 54:27:8d:00:00:02. Port 2 bounds to MAC 54:27:8d:00:00:02.

Frame forwarding.
The frame received from pseudo port. Dest Address 54:27:8d:00:00:00 Src Address 54:27:8d:00:00:f0. Frame forwarding to port 0.
The frame received from pseudo port. Dest Address 54:27:8d:00:00:02 Src Address 54:27:8d:00:00:f0. Frame forwarding to port 2.