Hardware requirements#
Mini/micro USB cable
FRDM-IMXRT1186 board
Personal Computer
Board settings#
Change Jumper J27 from 1-2 to 2-3
Probe the signal using an oscilloscope
At J51-8
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
Compare output example
~~~~~~~~~~~~~~~~~~~~~~~