Hardware requirements#
Micro USB cable
evkmimxrt595 board
Personal Computer
USB to serial converter
One of the following modules:
AzureWave AW-CM358MA.M2
AzureWave AW-CM510MA.M2
Embedded Artists 1XK M.2 Module (EAR00385)
Embedded Artists 1ZM M.2 Module (EAR00364)
Embedded Artists 2EL M.2 Module (Rev-A1) - direct M2 connection.
Board settings#
Before building the example application select Wi-Fi module macro in the app_bluetooth_config.h. (see #define WIFI_
Jumper settings for RT595 (enables external 5V supply):#
connect J39 with external power JP4 1-2 J27 1 - TX of USB to serial converter J27 2 - RX of USB to serial converter
Debug console UART is configured to use pins of J27, connect the board with PC by USB/UART converter:
board UART RX (pin 1 on J27) - connect to TX pin on converter
board UART TX (pin 2 on J27) - connect to RX pin on converter
board GND (pin 7 on J29) - connect to GND pin on converter
Murata Solution Board settings#
Embedded Artists M.2 module resource page: https://www.embeddedartists.com/m2 Embedded Artists 1XK module datasheet: https://www.embeddedartists.com/doc/ds/1XK_M2_Datasheet.pdf Embedded Artists 1ZM module datasheet: https://www.embeddedartists.com/doc/ds/1ZM_M2_Datasheet.pdf Embedded Artists 2EL module datasheet: https://www.embeddedartists.com/doc/ds/2EL_M2_Datasheet.pdf
AzureWave Solution Board settings#
The hardware should be reworked according to the Hardware Rework Guide for MIMXRT595-EVK and Murata M.2 Module in document Hardware Rework Guide for EdgeFast BT PAL. The hardware should be reworked according to the Hardware Rework Guide for MIMXRT595-EVK and AW-AM510MA in document Hardware Rework Guide for EdgeFast BT PAL. The hardware should be reworked according to the Hardware Rework Guide for MIMXRT595-EVK and AW-CM358MA in document Hardware Rework Guide for EdgeFast BT PAL.
Note: To ensure that the LITTLEFS flash region has been cleaned, all flash sectors need to be erased before downloading example code. After downloaded binary into qspiflash and boot from qspiflash directly, please reset the board by pressing SW3 or power off and on the board to run the application.