Hardware requirements#
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the PUF driver example in the terminal window (the key value will vary):
PUF Peripheral Driver Example
Reconstructed intrinsic key = 5a 66 b8 11 41 2e 74 4f fb 33 46 80 9c 9f 5c 1a
Example end.