MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the hello world demo in the terminal window:

IEE APC Demo started

Set up IEE APC regions
Enable IEE APC regions
IEE init
Load keys into IEE
Write plain text data to be encrypted at addess 0x20500000:
0x48656c6c6f576f726c64506c61696e21 -> "HelloWorldPlain!"

Turn off ecryption/decryption

Read encrypted data, From address 0x20500000 :
0x65e9320c8d12c25f282c1a4761e5955 -> "eé2ÈÑ,%òÁ¤vYU"

Turn on ecryption/decryption

Read decrypted data, From address 0x20500000:
0x48656c6c6f576f726c64506c61696e21 -> "HelloWorldPlain!"


IEE & IEE_APC demo End.