Hardware requirements#
Mini/micro USB cable
EVK-MIMXRT1160 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
TMPSNS driver example.
The chip initial temperature is 23.4 ℃.
The chip temperature has reached high temperature that is 27.2 ℃.
The chip will to be waiting a desired cool down temperature .
The chip temperature has reached high temperature that is 27.2 ℃.
The chip will to be waiting a desired cool down temperature .
The chip temperature has reached high temperature that is 27.2 ℃.
The chip will to be waiting a desired cool down temperature .
......
~~~~~~~~~~~~~~~~~~~~~~~
Note 1:
To run this exmaple successfully, you should heating the chip outside, such as blowing heating.
Note 2:
To debug in qspiflash, following steps are needed:
1. Select the flash target and compile.
3. Set the SW1: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J11.
4. Start debugging in IDE.
- Keil: Click "Download (F8)" to program the image to qspiflash first then clicking "Start/Stop Debug Session (Ctrl+F5)" to start debugging.