Hardware requirements#
Micro USB cable
evkmimxrt1040 board
Personal Computer
One of the following modules:
AzureWave AW-CM358MA.M2
AzureWave AW-CM510MA.M2
Embedded Artists 1XK M.2 Module (EAR00385)
Embedded Artists 1ZM M.2 Module (EAR00364)
Embedded Artists 2LL M.2 Module (EAR00500)
Board settings#
Before building the example application select Wi-Fi module macro in the app_bluetooth_config.h. (see #define WIFI_
Jumper settings for RT1040 (enables external 5V supply):#
connect J45 with external power SW6 2-3 J40 1-2
Murata Solution Board settings#
Embedded Artists M.2 module resource page: https://www.embeddedartists.com/m2 Embedded Artists 1XK module datasheet: https://www.embeddedartists.com/doc/ds/1XK_M2_Datasheet.pdf Embedded Artists 1ZM module datasheet: https://www.embeddedartists.com/doc/ds/1ZM_M2_Datasheet.pdf Embedded Artists 2LL module datasheet: https://www.embeddedartists.com/wp-content/uploads/2024/12/2LL_M2_Datasheet.pdf
AzureWave Solution Board settings#
The hardware should be reworked according to the hardware rework guide for evkmimxrt1040 with Direct Murata M.2 Module in document Hardware Rework Guide for EdgeFast BT PAL.
Note: To ensure that the LITTLEFS flash region has been cleaned, all flash sectors need to be erased before downloading example code. After downloaded binary into qspiflash and boot from qspiflash directly, please reset the board by pressing SW7 or power off and on the board to run the application.