Hardware requirements#
Mini/micro USB cable
EVK-MIMXRT1010 board
Personal Computer
Board settings#
Matrix and Jumper settings for KPP:
row1 <—–> J57-6 row2 <—–> J57-8 row3 <—–> J57-18 col1 <—–> J57-12 col2 <—–> J57-10 col3 <—–> J57-20
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Connect the 3*3 matrix to the Jumpers mentioned above.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When you press any key on matrix, the log will show the right key you have pressed. If you press a key continuously, it will print “this was a long press” repeately. The log would be seen on the OpenSDA terminal like:
KPP Driver Example Start.
Key SW1 was pressed.
Key SW3 was pressed.
Key SW1 was released.
Key SW3 was released.
All keys released.
This was a long press.
This was a long press.
......
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.