Hardware requirements#
Micro USB cable
MIMX8MQ6-EVK board
J-Link Debug Probe
SD card with uboot
12V power supply
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Prepare an SD card with the prebuilt U-Boot image. Then, insert the SD card to the target board.
Connect a USB cable between the host PC and the J1701 USB port on the target board.
Connect 12V power supply and J-Link Debug Probe to the board, switch SW701 to power on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
Follow the output log, lock and unlock the sema4 gate in uboot. The whole log:
SEMA4 uboot example start
Lock sema4 gate in uboot using:
> mw.b 0x30ac0000 1 1
Unlock sema4 gate in uboot using:
> mw.b 0x30ac0000 0 1
SEMA4 uboot example success