Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

  • Headphone(OMTP standard)

  • CS42448 Audio board(Not necessary if use on board codec)

Board settings

For Audio board: 1.Insert AUDIO board into J23 if on board codec is not used

Prepare the Demo

Note: As the EVKCMIMXRT1060 support two codecs, a default on board WM8962 codec and another codec CS42448 on audio board, so to support both of the codecs, the example provide options to switch between the two codecs,

  • DEMO_CODEC_WM8962, set to 1 if wm8962 used

  • DEMO_CODEC_CS42448, set to 1 if cs42448 used Please do not set above macros to 1 together, as the demo support one codec only.

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board. Steps for WM8962:

  4. Insert the headphones into the headphone jack on MIMXRT1060-EVKC board (J101). Steps for CS42448:

  5. Insert the headphones into the headphone jack J6 on the audio board.

  6. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

Note: This demo outputs 1000HZ sine wave audio signal. When the demo runs successfully, you can hear the tone and the log would be seen on the OpenSDA terminal like:

SAI functional interrupt example started!

SAI functional interrupt example finished!