Hardware requirements#
Mini/micro USB cable
MIMXRT1170-EVK board
Personal Computer
RK055MHD091 panel or RK055AHD091 panel or RK055IQH091 panel
Board settings#
Connect the panel to J48 Connect 5V power to J43, set J38 to 1-2
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build the project, the project uses RK055MHD091 by default, to use other panels, set the coresponding panel DEMO_PANEL_xxx(without ‘_SUPPORT’) to y in prj.conf under board example folder before project generation. The supported panels can be found in examples_boards<board>\project_segments\display_support\Kconfig.prjseg. Or change the macro DEMO_PANEL in mcux_config.h of the project, which number represents which panel can be found in display_support.h and mcux_config.h
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs, you can see a cube object with each face having high render quality. The cube face assets are rendered from VG paths. The cube has a moving effect done using isometric projection.