Hardware requirements

  • Micro USB cable

  • MIMXRT1170-EVKB board

  • JLink Plus

  • 5V power supply

  • Personal Computer

  • RK055MHD091 panel or RK055AHD091 panel or RK055IQH091 panel or RaspberryPi panel

  • SD card

Board settings

  1. Connect the panel to J48. For RaspberryPi panel, connect the panel to J84, then connect the panel’s 5V pin to J85-1, GND pin to J85-2.

  2. Prepare the H264 files and save in SD card.

  3. Please make sure R136 is weld for GPIO card detect.

  4. Insert the SDCARD into card slot(J15).

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build the project, the project uses RK055MHD091 by default, to use other panels, set the coresponding panel DEMO_PANEL_xxx(without ‘_SUPPORT’) to y in prj.conf under board example folder before project generation. The supported panels can be found in examples_boards<board>\project_segments\display_support\Kconfig.prjseg. Or change the macro DEMO_PANEL in mcux_config.h of the project, which number represents which panel can be found in display_support.h and mcux_config.h

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

If this example runs correctly, pictures are shown in the lcd panel.