MCUXpresso SDK Documentation

Platform Library#

Overview#

Device platform library examples are device specific example which share the general build system mechanism for example creation and configuration. They are all located in examples_int repo folder.

Take MIMXRT1176 as an example, the cmd to run is like:

west build --device MIMXRT1176 examples_int/platformlib -Dcore_id=cm7 --enable-all-drivers -p
west build --device MIMXRT1176 examples_int/platformlib -Dcore_id=cm7 --enable-all-drivers -p --toolchain=iar
west build --device MIMXRT1176 examples_int/platformlib -Dcore_id=cm7 --enable-all-drivers -p --toochain=mdk

CMakeLists.txt#

The platform library example CMakeLists.txt is located in examples_int/platformlib.

Here is its contents:

cmake_minimum_required(VERSION 3.30.0)

include(${SdkRootDirPath}/cmake/extension/mcux.cmake)

# PROJECT_DEVICE_PORT_PATH instead of PROJECT_BOARD_PORT_PATH
# PROJECT_TYPE must be LIBRARY
project(mcux_platformlib LANGUAGES C CXX ASM PROJECT_DEVICE_PORT_PATH examples_int/_devices/${device}/platformlib PROJECT_TYPE LIBRARY)

# Unlike common board examples, it doesn't add the root CMakeLists.txt as entry point. Instead, it only uses device cmakes and driver cmakes.
# device cmakes
mcux_add_cmakelists(${SdkRootDirPath}/${device_root}/${soc_portfolio}/${soc_series}/${device})
# driver cmakes
mcux_load_all_cmakelists_in_directory(${SdkRootDirPath}/drivers)

# example port/reconfiguration for device
include(${SdkRootDirPath}/examples_int/_devices/${device}/platformlib/${multicore_foldername}/reconfig.cmake OPTIONAL)

Kconfig#

Overview#

Platform library example has its own Kconfig only “source” drivers and device.

mainmenu "Mcux platform library"

source "${SdkRootDirPath}/drivers/Kconfig"

source "${SdkRootDirPath}/devices/Kconfig"

Driver selection#

--enable-all-drivers feature is provided to automatically selected all depended drivers for designated device based on the Kconfig.chip IP information. It will add default y for all Kconfig symbols starting with MCUX_COMPONENT_driver prefix if there is default provided so that if the driver dependency is satisfied for the device, then it will be added into build tree.

The common prj.conf for platform library example sets CMSIS, system and startup components to y:

CONFIG_MCUX_COMPONENT_device.CMSIS=y
CONFIG_MCUX_COMPONENT_device.system=y
CONFIG_MCUX_COMPONENT_device.startup=y

If you want to disable or enable some drivers additionally, you can still use the device port prj.conf to do it.

GUI Project Generation#

Platform library example support GUI project generation. The cmd is like

west build --device MIMXRT1176 examples_int/platformlib -Dcore_id=cm7 --enable-all-drivers -p --toochain=iar -t guiproject

The common IDE.yml only sets the project template:

mdk:
  project_language: cpp
  project-templates:
    - scripts/guigenerator/templates/mdk/lib_generic_arm/libgeneric_armclang.uvprojx
  config:
    __common__:
      cp-define:
        ${CONFIG_MCUX_TOOLCHAIN_MDK_CPU_IDENTIFIER}: NXP

iar:
  project_language: auto
  project-templates:
    - scripts/guigenerator/templates/iar/lib_generic_arm/libgeneric.ewp
    - scripts/guigenerator/templates/iar/lib_generic_arm/libgeneric.eww
  config:
    __common__:
      cp-define:
        ${CONFIG_MCUX_TOOLCHAIN_IAR_CPU_IDENTIFIER}: NXP ${CONFIG_MCUX_TOOLCHAIN_IAR_CPU_IDENTIFIER}
      cx-flags:
        - -e # enable IAR extension, if no cpp file included, gui project cant get this flag from ninja

If customization is needed for certain device, then additional IDE.yml could be provided in the device port folders just like common board example.

Example.yml#

The device example.yml content is a little different from board example:

# yaml-language-server: $schema=../../scripts/data_schema/example_description_schema.json
mcux_platformlib:
  section-type: library
  contents:
    meta_path: examples_int/platformlib
    project-root-path: ""
    document:
      name: mcux_platformlib${core_id_suffix_name}
      device_example: true
      category: platformlib
      brief: platformlib containing all base SDK drivers
      extra_build_args:
        - "--enable-all-drivers"
    toolchains: # specify the basic toolchains and targets
    - +armgcc@debug
    - +armgcc@release
    - +iar@debug
    - +iar@release
    - +mdk@debug
    - +mdk@release
  devices:
    MIMXRT1176@cm7: []

It uses the mcux_platformlib/contents/toolchains to specify the basic toolchains and build configurations it supports. Extra device specific toolchains and build configurations are specified in devices hash data just like boards for board examples.