MCUXpresso SDK Documentation

How to determine COM port

How to determine COM port#

This section describes the steps to determine the debug COM port number of your NXP hardware development platform.

  1. Linux: The serial port can be determined by running the following command after the USB Serial is connected to the host:

    $ dmesg | grep "ttyUSB"
    [503175.307873] usb 3-12: cp210x converter now attached to ttyUSB0
    [503175.309372] usb 3-12: cp210x converter now attached to ttyUSB1
    

    There are two ports, one is Cortex-A core debug console and the other is for Cortex M33.

  2. Windows: To determine the COM port, open Device Manager. Click the Start menu and type Device Manager in the search bar.

    |

|

  1. In the Device Manager, expand the Ports (COM & LPT) section to view the available ports. The COM port names are different for all the NXP boards.

    1. USB-UART interface

      |

|