Build a TrustZone example application#
This section describes the steps required to configure MCUXpresso IDE to build, run, and debug TrustZone example applications. The TrustZone version of the hello_world example application targeted for the MIMXRT685-EVK hardware platform is used as an example, though these steps can be applied to any TrustZone example application in the MCUXpresso SDK.
TrustZone examples are imported into the workspace in a similar way as single core applications. When the SDK zip package for MIMXRT685-EVK is installed and available in the Installed SDKs view, click Import SDK example(s)… on the Quickstart Panel. In the window that appears, expand the MIMXRT600 folder and select MIMXRT685S. Then, select evkmimxrt685 and click Next.
|

|
Expand the
trustzone_examples/folder and selecthello_world_s. Because TrustZone examples are linked together, the non-secure project is automatically imported with the secure project, and there is no need to select it explicitly. Then, click Finish.|

|
Now, two projects should be imported into the workspace. To start building the TrustZone application, highlight the
evkmimxrt685\_hello\_world\_sproject (TrustZone master project) in the Project Explorer. Then, choose the appropriate build target, Debug, or Release, by clicking the downward facing arrow next to the hammer icon, as shown in Figure 3. For this example, select the Debug target.
|
|
The project starts building after the build target is selected. It is requested to build the application for the secure project first, because the non-secure project must know the secure project since CMSE library when running the linker. It is not possible to finish the non-secure project linker when the secure project since CMSE library is not ready.
**Note:** When the **Release** build is requested, it is necessary to change the build configuration of both the secure and non-secure application projects first. To do this, select both projects in the Project Explorer view by clicking to select the first project, then using shift-click or control-click to select the second project. Right click in the Project Explorer view to display the context-sensitive menu and select **Build Configurations** \> **Set Active** \>**Release**. This is also possible by using the menu item of **Project** \> **Build Configuration** \>**Set Active** \>**Release**. After switching to the **Release** build configuration. Build the application for the secure project first.
|
|
Parent topic:Run a demo using MCUXpresso IDE