MCUXpresso SDK Documentation

Build an example application

Build an example application#

Do the following steps to build the hello_world example application..

  1. Open the desired demo application workspace. Most example application workspace files can be located using the following path:

    <install_dir>/boards/<board_name>/<example_type>/<application_name>/iar
    

    Using the frdmmcxw72 hardware platform as an example, the hello_world workspace is located in:

    <install_dir>/boards/frdmmcxw72/demo_apps/hello_world/iar/hello_world.eww
    

    Other example applications may have additional folders in their path.

  2. Select the desired build target from the drop-down menu.

    For this example, select hello_worlddebug.

  3. To build the demo application, click Make, highlighted in red in Figure 2.

![](../images/iar_build_the_demo_application.jpg "Build the demo application")
  1. The build completes without errors.

Parent topic:Running a demo application using IAR