Functions
The following Commissioning cluster function is provided:
eCLD_CommissioningClusterCreateCommissioning
teZCL_Status eCLD_CommissioningClusterCreateCommissioning(
tsZCL_ClusterInstance *psClusterInstance,
bool_t bIsServer,
tsZCL_ClusterDefinition *psClusterDefinition,
void *pvEndPointSharedStructPtr,
uint8 *pu8AttributeControlBits,
tsCLD_CommissioningCustomDataStructure
*psCustomDataStructure);
Description
This function creates an instance of the Commissioning cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.
The function should only be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function will create a Commissioning cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions. For more details of creating cluster instances on custom endpoints, refer to Appendix D.
Note: This function must not be called for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function from those described in the ZigBee Devices User Guide
Note: (JNUG3131).
When used, this function must be called after the stack has been started and after the ZCL has been initialized.
The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length is automatically adjusted by the compiler using the following declaration:
uint8 au8CommissioningAttributeControlBits
[(sizeof(asCLD_CommissioningClusterAttributeDefinitions) / sizeof(tsZCL_AttributeDefinition))];
Parameters
psClusterInstance Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initialising individual structure fields.
bIsServer Type of cluster instance (server or client) to be created:
TRUE - server
FALSE - client
psClusterDefinition Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the Commissioning cluster. This parameter can refer to a pre-filled structure called
sCLD_Commissioningwhich is provided in the Commissioning.h file.pvEndPointSharedStructPtr Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type
tsCLD_Commissioningwhich defines the attributes of Commissioning cluster. The function initializes the attributes with default values.pu8AttributeControlBits Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above). For a cluster client, set this pointer to NULL.
psCustomDataStructure Pointer to a structure containing the storage for internal functions of the cluster (see Section 43.9.5)
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions
eCLD_CommissioningCommandRestartDeviceSend
teZCL_Status eCLD_CommissioningCommandRestartDeviceSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber, tsCLD_Commissioning_RestartDevicePayload *psPayload);
Description
This function can be used on a Commissioning cluster client to send a Restart Device command to a cluster server on a remote device. This command is used to run the start-up procedure with a new set of values for the Start-up Parameters attributes (these values must already be installed). The new values may be implemented immediately or after a specified delay with an optional jitter.
When the command arrives, a ZCL custom event will be generated and the request should be handled by the user-defined callback function for the endpoint on which the application is located (see Section 43.6). Before running the start-up procedure or starting the countdown (for the delay), the server will send a Restart Device Response to the requesting client, where a ZCL custom event will be generated.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress Pointer to a structure holding the address of the node to which the request is sent
pu8TransactionSequenceNumber Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
psPayload Pointer to a structure containing the payload for this message (see Section 43.9.2)
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions
eCLD_CommissioningCommandSaveStartupParamsSend
teZCL_Status eCLD_CommissioningCommandSaveStartupParamsSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber
tsCLD_Commissioning_ModifyStartupParametersPayload *psPayload);
Description
This function can be used on a Commissioning cluster client to send a Save Start-up Parameters command to a cluster server on a remote device. This command instructs the server to locally save a set of values for the attributes of the Start-up Parameters attribute set. A device can store different sets of start-up parameters (in non-volatile memory), with each set being referenced using an index number. This index number must be specified and if a set has already been stored with the same index number then the stored values will be over-written with the new values.
It is the responsibility of the user application on the device hosting the server to implement the command. When the command arrives, a ZCL custom event will be generated and the request should be handled by the user-defined callback function for the endpoint on which the application is located (see Section 43.6). The server will automatically send a Save Start-up Parameters Response to the client, where a ZCL custom event will be generated.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress Pointer to a structure holding the address of the node to which the request is sent
pu8TransactionSequenceNumber Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
psPayload Pointer to a structure containing the payload for this message (see Section 43.9.3)
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions
eCLD_CommissioningCommandRestoreStartupParamsSend
teZCL_Status eCLD_CommissioningCommandRestoreStartupParamsSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber, tsCLD_Commissioning_*psPayload)
Description
This function can be used on a Commissioning cluster client to send a Restore Start-up Parameters command to a cluster server on a remote device. This command instructs the server to load a saved set of values for the attributes of the Start-up Parameters attribute set. The index of the required set of Start-up Parameters must be specified in the command payload. Note that the command does not instruct the server to implement the loaded values using the start-up procedure - a Restart Device command is required to do this.
It is the responsibility of the user application on the device hosting the server to implement the command. When the command arrives, a ZCL custom event will be generated and the request should be handled by the user-defined callback function for the endpoint on which the application is located (see Section 43.6). The server will automatically send a Restore Start-up Parameters Response to the client, where a ZCL custom event will be generated.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress Pointer to a structure holding the address of the node to which the request is sent
pu8TransactionSequenceNumber Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
psPayload Pointer to a structure containing the payload for this message (see Section 43.9.3)
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions
eCLD_CommissioningCommandResetStartupParamsSend
teZCL_Status eCLD_CommissioningCommandResetStartupParamsSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber, tsCLD_*psPayload);
Description
This function can be used on a Commissioning cluster client to send a Reset Start-up Parameters command to a cluster server on a remote device. This command instructs the server to set the current Start-up Parameters to their default values. It is also possible to set one or all of any saved sets of Start-up Parameters to the defaults. The command can also be used to delete a specified set of saved Start-up Parameters.
It is the responsibility of the user application on the device hosting the server to implement the command. When the command arrives, a ZCL custom event will be generated and the request should be handled by the user-defined callback function for the endpoint on which the application is located (see Section 43.6). The server will automatically send a Reset Start-up Parameters Response to the client, where a ZCL custom event will be generated.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress Pointer to a structure holding the address of the node to which the request is sent
pu8TransactionSequenceNumber Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
psPayload Pointer to a structure containing the payload for this message (see Section 43.9.3)
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions
eCLD_CommissioningCommandModifyStartupParamsSend
teZCL_Status eCLD_CommissioningCommandModifyStartupParamsSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_Commissioning_ModifyStartupParametersPayload *psPayload,
teCLD_Commissioning_Command eCLD_Commissioning_Command);
Description
This function can be used on a Commissioning cluster client to send a command to modify a set of values for the Start-up Parameters attributes in the cluster server on a remote device. One of four commands can be specified and sent, as listed and described in the table below:
Command |
Description |
|---|---|
Restart Device |
Used to run the start-up procedure with the current set of values for the Start-up Parameters attributes, as described for the function eCLD_Com-missioningCommandRestartDeviceSend(). These values may have been loaded using the Restore Start-up Parameters or Reset Start-up Parameters command. |
Save Start-up Parameters |
Used to save the current set of Start-up Parameter values with the speci-fied index, as described for the function eCLD_CommissioningCom-mandSaveStartupParamsSend(). |
Restore Start-up Parameters |
Used to load the saved set of Start-up Parameter values with the specified index, such that these values become the current Start-up Parameter val-ues, as described for the function eCLD_CommissioningCommandRe-storeStartupParamsSend(). Note that these values are not implemented, which requires a Restart Device command. |
Reset Start-up Parameters |
Used to reset the current Start-up Parameters to their defaults. One or all of any stored sets of Start-up Parameter values can also be reset to the defaults, as described for the function eCLD_CommissioningComman-dResetStartupParamsSend(). The command can also be used to delete a particular set of stored Start-up Parameters. |
It is the responsibility of the user application on the device hosting the server to implement the command. When the command arrives, a ZCL custom event will be generated and the request should be handled by the user-defined callback function for the endpoint on which the application is located (see Section 43.6). The server will automatically send a response for the relevant command to the client, where a ZCL custom event will be generated.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress Pointer to a structure holding the address of the node to which the request is sent
pu8TransactionSequenceNumber Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
psPayload Pointer to a structure containing the payload for this message (see Section 43.9.3)
eCLD_Commissioning_Command Type of command to send, one of:
E_CLD_COMMISSIONING_CMD_RESTART_DEVICE
E_CLD_COMMISSIONING_CMD_SAVE_STARTUP_PARAMS
E_CLD_COMMISSIONING_CMD_RESTORE_STARTUP_PARAMS
E_CLD_COMMISSIONING_CMD_RESET_STARTUP_PARAMS
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions
eCLD_CommissioningSetAttribute
teZCL_Status eCLD_CommissioningSetAttribute(
uint8 u8SourceEndPointId,
teCLD_Commissioning_AttributeSet eAttributeSet,
void *vptrAttributeSetStructure);
Description {
This function can be used on a Commissioning cluster server to write values to a particular attribute set of the Commissioning cluster.
Parameters
u8SourceEndPointId Number of the local endpoint through which to issue the request.
eAttributeSet Enumeration indicating attribute set to write to, one of:
E_CLD_COMMISSIONING_ATTR_SET_STARTUP_PARAMS
E_CLD_COMMISSIONING_ATTR_SET_JOIN_PARAMS
E_CLD_COMMISSIONING_ATTR_SET_ENDDEVICE_PARAMS
E_CLD_COMMISSIONING_ATTR_SET_CONCENTRATOR_PARAMS
vptrAttributeSetStructure Pointer to a structure containing the new values for the attribute set - the relevant structures are detailed in Section 43.2
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions
Parent topic:Commissioning Cluster