MCUXpresso SDK Documentation

Commissioning Events

Commissioning Events#

The Commissioning cluster has its own events that are handled through the callback mechanism outlined in Chapter 3. If a device uses this cluster then application-specific Commissioning event handling must be included in the user-defined callback function for the associated endpoint, where this callback function is registered through the relevant endpoint registration function. This callback function will then be invoked when a Commissioning event occurs and needs the attention of the application.

For a Commissioning event, the eEventType field of the tsZCL_CallBackEvent structure is set to E_ZCL_CBET_CLUSTER_CUSTOM. This event structure also contains an element sClusterCustomMessage, which is itself a structure containing a field pvCustomData. This field is a pointer to the following tsCLD_CommissioningCallBackMessage structure (fully detailed in Section43.9.6).

typedef struct
{
    uint8                      u8CommandId;
    union
    {
        tsCLD_Commissioning_RestartDevicePayload                    
                              *psRestartDevicePayload;
        tsCLD_Commissioning_ModifyStartupParametersPayload          
                              *psModifyStartupParamsPayload; 
    } uReqMessage;
    union
    {
        tsCLD_Commissioning_ResponsePayload                         
                              *psCommissioningResponsePayload; 
    } uRespMessage;
} tsCLD_CommissioningCallBackMessage;

When a Commissioning event occurs, one of a number of command types could have been received. The relevant command type is specified through the u8CommandId field of the tsCLD_CommissioningCallBackMessage structure. The possible command types are detailed below.

The table below details the command types that can be received by the cluster server.

u8CommandId Enumeration

Description

E_CLD_COMMISSIONING_CMD_RESTART_DEVICE

A Restart Device command has been received

E_CLD_COMMISSIONING_CMD_SAVE_STARTUP_PARAMS

A Save Start-up Parameters command has been received

E_CLD_COMMISSIONING_CMD_RESTORE_STARTUP_PARAMS

A Restore Start-up Parameters command has been received

E_CLD_COMMISSIONING_CMD_RESET_STARTUP_PARAMS

A Reset Start-up Parameters command has been received

The table below details the command types that can be received by the cluster client.

u8CommandId Enumeration

Description

E_CLD_COMMISSIONING_CMD_RESTART_DEVICE

A Restart Device response has been received

E_CLD_COMMISSIONING_CMD_SAVE_STARTUP_PARAMS

A Save Start-up Parameters response has been received

E_CLD_COMMISSIONING_CMD_RESTORE_STARTUP_PARAMS

A Restore Start-up Parameters response has been received

E_CLD_COMMISSIONING_CMD_RESET_STARTUP_PARAMS

A Reset Start-up Parameters response has been received

Parent topic:Commissioning Cluster