MCUXpresso SDK Documentation

tsCLD_Commissioning_ModifyStartupParametersPayload

tsCLD_Commissioning_ModifyStartupParametersPayload#

The following structure contains the payload of the following commands: Save Start-up Parameters, Restore Start-up Parameters and Reset Start-up Parameters.

typedef struct
{
    zbmap8                  u8Options;
    uint8                   u8Index;
} tsCLD_Commissioning_ModifyStartupParametersPayload;

where:

u8Options is an 8-bit bitmap specifying the required reset options for the Reset Start-up Parameters command (it is not used by the other commands):

Bits

Option

Description

0

Reset Current

Determines whether the current Start-up Parameters will be reset to their default values:

  • 1: Reset to default values

  • 0: Do not reset (remain unchanged)

| |1|Reset All|Determines whether all stored Start-up Parameter sets will be reset to their default values:

  • 1: Reset all stored Start-up Parameter sets

  • 0: Reset the stored Start-up Parameter set with specified index

| |2|Erase Index|Determines whether the stored Start-up Parameter set with speci-fied index will be erased:

  • 1: Erase Start-up Parameter set with specified index

  • 0: Do not erase Start-up Parameter set with specified index

| |3-7|-|Reserved|

u8Index is the index of the saved Start-up Parameter set to which actions specified in u8Options relate (this index is ignored if no actions are specified).

Parent topic:Structures