MCUXpresso SDK Documentation

eCLD_CommissioningCommandResetStartupParamsSend

eCLD_CommissioningCommandResetStartupParamsSend#

teZCL_Status eCLD_CommissioningCommandResetStartupParamsSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber, tsCLD_*psPayload);

Description#

This function can be used on a Commissioning cluster client to send a Reset Start-up Parameters command to a cluster server on a remote device. This command instructs the server to set the current Start-up Parameters to their default values. It is also possible to set one or all of any saved sets of Start-up Parameters to the defaults. The command can also be used to delete a specified set of saved Start-up Parameters.

It is the responsibility of the user application on the device hosting the server to implement the command. When the command arrives, a ZCL custom event will be generated and the request should be handled by the user-defined callback function for the endpoint on which the application is located (see Section 43.6). The server will automatically send a Reset Start-up Parameters Response to the client, where a ZCL custom event will be generated.

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId        Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values

  • u8DestinationEndPointId        Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP

  • psDestinationAddress        Pointer to a structure holding the address of the node to which the request is sent

  • pu8TransactionSequenceNumber        Pointer to a location to receive the Transaction Sequence Number (TSN) of the request

  • psPayload        Pointer to a structure containing the payload for this message (see Section 43.9.3)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_INVALID_VALUE

Parent topic:Functions