MCUXpresso SDK Documentation

Functions#

The following Thermostat cluster functions are provided:

eCLD_ThermostatCreateThermostat#

teZCL_Status eCLD_ThermostatCreateThermostat(
    tsZCL_ClusterInstance *psClusterInstance,
    bool_t bIsServer,
    sZCL_ClusterDefinition *psClusterDefinition,
    void *pvEndPointSharedStructPtr,
    uint8 *pu8AttributeControlBits,
    tsCLD_ThermostatCustomDataStructure
    psCustomDataStructure);

Description#

This function creates an instance of the Thermostat cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.

The function should only be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function will create a Thermostat cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions.

Note: This function must not be called for an endpoint on which a standard ZigBee device (e.g. the Thermostat device) will be used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function.

When used, this function must be the first Thermostat cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.

The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length should therefore equate to the total number of attributes supported by the Thermostat cluster.

The function initializes the array elements to zero.

Parameters#

  • psClusterInstance        Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initialising individual structure fields.

  • bIsServer         Type of cluster instance (server or client) to be created:

  • TRUE - server

  • FALSE - client

  • psClusterDefinition        Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the Thermostat cluster. This parameter can refer to a pre-filled structure called sCLD_``Thermostat which is provided in the Thermostat.h file.

  • pvEndPointSharedStructPtr        Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type tsCLD_``Thermostat which defines the attributes of Thermostat cluster. The function initializes the attributes with default values.

  • pu8AttributeControlBits        Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above).

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_INVALID_VALUE

Parent topic:Functions

eCLD_ThermostatSetAttribute#

teZCL_Status eCLD_ThermostatSetAttribute(
    uint8 u8SourceEndPointId,
    uint8 u8AttributeId,
    int16 i16AttributeValue);

Description#

This function can be used on a Thermostat cluster server to update the Thermostat attributes - specifically to write a value to one of the following attributes:

i16LocalTemperature
i16OccupiedCoolingSetpoint
i16OccupiedHeatingSetpoint

The function first checks whether the value to be written falls within the valid range for the relevant attribute. If not, it returns with status E_ZCL_ERR_INVALID_VALUE. If the server attempts to write to an attribute other than those specified above, the function returns with status E_ZCL_DENY_ATTRIBUTE_ACCESS. If the cluster does not exist, it returns with status E_ZCL_ERR_CLUSTER_NOT_FOUND.

Parameters#

  • u8SourceEndPointId        Number of the endpoint on which the Thermostat cluster resides

  • u8AttributeId         Identifier of attribute to be updated, one of:

  • E_CLD_THERMOSTAT_ATTR_ID_LOCAL_TEMPERATURE

  • E_CLD_THERMOSTAT_ATTR_ID_OCCUPIED_COOLING_SETPOINT

  • E_CLD_THERMOSTAT_ATTR_ID_OCCUPIED_HEATING_SETPOINT

  • i16AttributeValue        Value to be written to attribute

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_INVALID_VALUE

  • E_ZCL_DENY_ATTRIBUTE_ACCESS

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

Parent topic:Functions

eCLD_ThermostatStartReportingLocalTemperature#

teZCL_Status eCLD_ThermostatStartReportingLocalTemperature(
    uint8 u8SourceEndPointId,
    uint8 u8DstEndPointId,
    uint64 u64DstAddr,
    uint16 u16MinReportInterval,
    uint16 u16MaxReportInterval,
    int16 i16ReportableChange);

Description#

This function can be used on a Thermostat cluster server to start automatic reporting of the measured local temperature to a cluster client. The change to be reported can be configured through this function. Reports is sent regularly (but not periodically), within the specified maximum and minimum time-intervals between consecutive reports.

Parameters#

  • u8SourceEndPointId        Number of the local endpoint on which the Thermostat cluster server resides

  • u8DstEndPointId        Number of the endpoint to which reports are to be sent on the destination node

  • u64DstAddr                IEEE/MAC address of destination node

  • u16MinReportInterval                Minimum time-interval, in seconds, between reports

  • u16MaxReportInterval                Maximum time-interval, in seconds, between reports

  • i16ReportableChange                Specifies the change to be reported

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

Parent topic:Functions

eCLD_ThermostatCommandSetpointRaiseOrLowerSend#

teZCL_Status eCLD_ThermostatCommandSetpointRaiseOrLowerSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_Thermostat_SetpointRaiseOrLowerPayload
*psPayload);

Description#

This function can be used on a Thermostat cluster client to send a ‘Setpoint Raise Or Lower’ command to the cluster server. This command is used to increase or decrease the heating setpoint and/or cooling setpoint by requesting a change to the values of the attribute i16OccupiedHeatingSetpoint and/or the attribute i16OccupiedCoolingSetpoint. The relevant setpoint(s) and the required temperature change are specified in the command payload structure tsCLD_Thermostat_SetpointRaiseOrLowerPayload (see Section 33.9.3).

A pointer must be specified to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request.

Parameters#

  • u8SourceEndPointId                Number of the local endpoint through which the request is sent

  • u8DestinationEndPointId                Number of the remote endpoint to which the request is sent

  • psDestinationAddress                Pointer to a structure containing the address of the remote node to which the request is sent

  • pu8TransactionSequenceNumber                Pointer to a location to store the Transaction Sequence Number (TSN) of the request

  • psPayload        Pointer to the command payload (see Section33.9.3)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

Parent topic:Functions

Parent topic:Thermostat Cluster