MCUXpresso SDK Documentation

eCLD_ThermostatSetAttribute

eCLD_ThermostatSetAttribute#

teZCL_Status eCLD_ThermostatSetAttribute(
    uint8 u8SourceEndPointId,
    uint8 u8AttributeId,
    int16 i16AttributeValue);

Description#

This function can be used on a Thermostat cluster server to update the Thermostat attributes - specifically to write a value to one of the following attributes:

i16LocalTemperature
i16OccupiedCoolingSetpoint
i16OccupiedHeatingSetpoint

The function first checks whether the value to be written falls within the valid range for the relevant attribute. If not, it returns with status E_ZCL_ERR_INVALID_VALUE. If the server attempts to write to an attribute other than those specified above, the function returns with status E_ZCL_DENY_ATTRIBUTE_ACCESS. If the cluster does not exist, it returns with status E_ZCL_ERR_CLUSTER_NOT_FOUND.

Parameters#

  • u8SourceEndPointId        Number of the endpoint on which the Thermostat cluster resides

  • u8AttributeId         Identifier of attribute to be updated, one of:

  • E_CLD_THERMOSTAT_ATTR_ID_LOCAL_TEMPERATURE

  • E_CLD_THERMOSTAT_ATTR_ID_OCCUPIED_COOLING_SETPOINT

  • E_CLD_THERMOSTAT_ATTR_ID_OCCUPIED_HEATING_SETPOINT

  • i16AttributeValue        Value to be written to attribute

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_INVALID_VALUE

  • E_ZCL_DENY_ATTRIBUTE_ACCESS

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

Parent topic:Functions