MCUXpresso SDK Documentation

eCLD_ThermostatStartReportingLocalTemperature

eCLD_ThermostatStartReportingLocalTemperature#

teZCL_Status eCLD_ThermostatStartReportingLocalTemperature(
    uint8 u8SourceEndPointId,
    uint8 u8DstEndPointId,
    uint64 u64DstAddr,
    uint16 u16MinReportInterval,
    uint16 u16MaxReportInterval,
    int16 i16ReportableChange);

Description#

This function can be used on a Thermostat cluster server to start automatic reporting of the measured local temperature to a cluster client. The change to be reported can be configured through this function. Reports is sent regularly (but not periodically), within the specified maximum and minimum time-intervals between consecutive reports.

Parameters#

  • u8SourceEndPointId        Number of the local endpoint on which the Thermostat cluster server resides

  • u8DstEndPointId        Number of the endpoint to which reports are to be sent on the destination node

  • u64DstAddr                IEEE/MAC address of destination node

  • u16MinReportInterval                Minimum time-interval, in seconds, between reports

  • u16MaxReportInterval                Maximum time-interval, in seconds, between reports

  • i16ReportableChange                Specifies the change to be reported

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

Parent topic:Functions