Structures#
Event Callback Message Structure#
For an Alarms event, the eEventType field of the tsZCL_CallBackEvent structure is set to E_ZCL_CBET_CLUSTER_CUSTOM. This event structure also contains an element sClusterCustomMessage, which is itself a structure containing a field pvCustomData. This field is a pointer to the following tsCLD_AlarmsCallBackMessage structure:
typedef struct
{
uint8 u8CommandId;
union
{
tsCLD_AlarmsResetAlarmCommandPayload *psResetAlarmCommandPayload;
tsCLD_AlarmsAlarmCommandPayload *psAlarmCommandPayload;
tsCLD_AlarmsGetAlarmResponsePayload *psGetAlarmResponse;
} uMessage;
} tsCLD_AlarmsCallBackMessage;
where:
u8CommandIdindicates the type of Alarms command that has been received by a cluster server or client, one of:E_CLD_ALARMS_CMD_RESET_ALARM (server event)
E_CLD_ALARMS_CMD_RESET_ALL_ALARMS (server event)
E_CLD_ALARMS_CMD_GET_ALARM (server event)
E_CLD_ALARMS_CMD_RESET_ALARM_LOG (server event)
E_CLD_ALARMS_CMD_ALARM (client event)
E_CLD_ALARMS_CMD_GET_ALARM_RESPONSE (client event)
uMessageis a union containing the command payload in the following form:psResetAlarmCommandPayloadis a pointer to a structure containing the Reset Alarm command payload - see Section 17.7.3.1psAlarmCommandPayloadis a pointer to a structure containing the Alarm notification payload - see Section 17.7.3.2psGetAlarmResponseis a pointer to a structure containing the Get Alarm response payload - see Section 17.7.4.1
For further information on the above events, refer to Section 17.5.
Parent topic:Structures
Custom Data Structure#
The Alarms cluster requires extra storage space to be allocated for use by internal functions. The structure definition for this storage is shown below:
typedef struct
{
DLIST lAlarmsAllocList;
DLIST lAlarmsDeAllocList;
tsZCL_ReceiveEventAddress sReceiveEventAddress;
tsZCL_CallBackEvent sCustomCallBackEvent;
tsCLD_AlarmsCallBackMessage sCallBackMessage;
tsCLD_AlarmsTableEntry
asAlarmsTableEntry[CLD_ALARMS_MAX_NUMBER_OF_ALARMS];
} tsCLD_AlarmsCustomDataStructure;
The fields are for internal use and no knowledge of them is required.
Parent topic:Structures
Custom Command Payloads#
This section contains the structures for the payloads of the Alarms cluster custom commands.
Reset Alarm Command Payload#
typedef struct
{
uint8 u8AlarmCode;
uint16 u16ClusterId;
} tsCLD_AlarmsResetAlarmCommandPayload;
where:
u8AlarmCodeis the code which identifies the type of alarm to be reset - these codes are cluster-specificu16ClusterIdis the Cluster ID of the cluster which generates the alarm to be reset
Parent topic:Custom Command Payloads
Alarm Notification Payload#
typedef struct
{
uint8 u8AlarmCode;
uint16 u16ClusterId;
} tsCLD_AlarmsAlarmCommandPayload;
where:
u8AlarmCodeis the code which identifies the type of alarm that has been generated - these codes are cluster-specificu16ClusterIdis the Cluster ID of the cluster which generated the alarm
Parent topic:Custom Command Payloads
Parent topic:Structures
Custom Response Payloads#
This section contains the structures for the payloads of the Alarms cluster custom responses.
Get Alarm Response Payload#
typedef struct
{
uint8 u8Status;
uint8 u8AlarmCode;
uint16 u16ClusterId;
uint32 u32TimeStamp;
} tsCLD_AlarmsGetAlarmResponsePayload;
where:
u8Statusindicates the result of the Get Alarm operation as follows:SUCCESS (0x01): An alarm entry is successfully retrieved from the Alarms table and its details are reported in the remaining fields (below)
NOT_FOUND (0x00): There were no alarm entries to be retrieved from the Alarms table and the remaining fields (below) are empty
u8AlarmCodeis the code which identifies the type of alarm reported - these codes are cluster-specificu16ClusterIdis the Cluster ID of the cluster which generated the alarmu32TimeStampis a timestamp representing the time (UTC) at which the alarm was generated (a value of 0XFFFFFFFF indicates that no timestamp is available for the alarm)
Parent topic:Custom Response Payloads
Parent topic:Structures
Alarms Table Entry#
The following structure contains the data for an entry of an Alarms table.
typedef struct
{
DNODE dllAlarmsNode;
uint8 u8AlarmCode;
uint16 u16ClusterId;
uint32 u32TimeStamp;
} tsCLD_AlarmsTableEntry;
where:
dllAlarmsNodeis for internal use and no knowledge of it is requiredu8AlarmCodeis the code which identifies the type of alarm - these codes are cluster-specificu16ClusterIdis the Cluster ID of the cluster which generated the alarmu32TimeStampis a timestamp representing the time (UTC) at which the alarm was generated (a value of 0XFFFFFFFF indicates that no timestamp is available for the alarm)
Parent topic:Structures
Parent topic:Alarms Cluster