Alarm Notification Payload#
typedef struct
{
uint8 u8AlarmCode;
uint16 u16ClusterId;
} tsCLD_AlarmsAlarmCommandPayload;
where:
u8AlarmCodeis the code which identifies the type of alarm that has been generated - these codes are cluster-specificu16ClusterIdis the Cluster ID of the cluster which generated the alarm
Parent topic:Custom Command Payloads