MCUXpresso SDK Documentation

Custom Response Payloads

Custom Response Payloads#

This section contains the structures for the payloads of the Alarms cluster custom responses.

Get Alarm Response Payload#

typedef struct
{
   uint8   u8Status;
   uint8   u8AlarmCode;
   uint16  u16ClusterId;
   uint32  u32TimeStamp;
} tsCLD_AlarmsGetAlarmResponsePayload;

where:

  • u8Status indicates the result of the Get Alarm operation as follows:

    • SUCCESS (0x01): An alarm entry is successfully retrieved from the Alarms table and its details are reported in the remaining fields (below)

    • NOT_FOUND (0x00): There were no alarm entries to be retrieved from the Alarms table and the remaining fields (below) are empty

  • u8AlarmCode is the code which identifies the type of alarm reported - these codes are cluster-specific

  • u16ClusterId is the Cluster ID of the cluster which generated the alarm

  • u32TimeStamp is a timestamp representing the time (UTC) at which the alarm was generated (a value of 0XFFFFFFFF indicates that no timestamp is available for the alarm)

Parent topic:Custom Response Payloads

Parent topic:Structures