Functions#
The following Alarms cluster functions are provided in the NXP implementation of the ZCL:
eCLD_AlarmsCreateAlarms#
teZCL_Status eCLD_AlarmsCreateAlarms(
tsZCL_ClusterInstance *psClusterInstance,
bool_t bIsServer,
tsZCL_ClusterDefinition *psClusterDefinition,
void *pvEndPointSharedStructPtr,
uint8 *pu8AttributeControlBits,
tsCLD_AlarmsCustomDataStructure
*psCustomDataStructure);
Description#
This function creates an instance of the Alarms cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.
The function is only called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function creates an Alarms cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions.
Note: This function is not called for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function.
When used, this function must be the first Alarms cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.
Parameters#
psClusterInstance:Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initializing individual structure fields.
bIsServer: Type of cluster instance (server or client) to be created:
TRUE - server
FALSE - client
psClusterDefinition: Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the Alarms cluster. This parameter can refer to a pre-filled structure called
sCLD_``Alarmswhich is provided in the Alarms.h file.pvEndPointSharedStructPtr: Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type
tsCLD_Alarmswhich defines the attributes of Alarms cluster. The function initializes the attributes with default values.pu8AttributeControlBits: Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above)
psCustomDataStructure: Pointer to a structure containing the storage for internal functions of the cluster (see Section 17.7.2)
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
Parent topic:Functions
eCLD_AlarmsCommandResetAlarmCommandSend#
teZCL_Status eCLD_AlarmsCommandResetAlarmCommandSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_AlarmsResetAlarmCommandPayload
*psPayload);
Description#
This function can be called on an Alarms cluster client to send a Reset Alarm command to a cluster server. This command requests that a specific alarm for a specific cluster is reset. The function may be called as the result of user input. The relevant alarm and cluster ID must be specified in the command payload (see Section 17.7.3.1).
On receiving the command, an E_CLD_ALARMS_CMD_RESET_ALARM event is generated on the cluster server to notify the application.
The function is only used to reset alarms that are not automatically reset when the alarm condition no longer exists.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent
psDestinationAddress: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
*psPayload: Pointer to a structure containing the payload for the command (see Section 17.7.3.1)
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_AlarmsCommandResetAllAlarmsCommandSend#
teZCL_Status eCLD_AlarmsCommandResetAllAlarmsCommandSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber);
Description#
This function can be called on an Alarms cluster client to send a Reset All Alarms command to a cluster server. This command requests that all alarms on the server device are reset. The function may be called as the result of user input.
On receiving the command, an E_CLD_ALARMS_CMD_RESET_ALL_ALARMS event is generated on the cluster server to notify the application.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent
psDestinationAddress: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_AlarmsCommandGetAlarmCommandSend#
teZCL_Status eCLD_AlarmsCommandGetAlarmCommandSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber);
Description#
This function can be used on an Alarms cluster client to send a Get Alarm command to a cluster server. This command requests information on the logged alarm with the earliest timestamp in the device’s Alarms table. As a result of this command, the retrieved entry is also deleted from the table.
The requested information is returned by the server in a Get Alarm response. When this response is received, an E_CLD_ALARMS_CMD_GET_ALARM_RESPONSE event is generated on the client.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent
psDestinationAddress: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_AlarmsCommandResetAlarmLogCommandSend#
teZCL_Status eCLD_AlarmsCommandResetAlarmLogCommandSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber);
Description#
This function can be called on an Alarms cluster client to send a Reset Alarm Log command to a cluster server. This command requests that the Alarms table on the server is cleared of all entries. The function may be called as the result of user input.
On receiving the command, an E_CLD_ALARMS_CMD_RESET_ALARM_LOG event is generated on the cluster server to notify the application but the ZCL automatically clears the Alarms table.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent
psDestinationAddress: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_AlarmsResetAlarmLog#
teZCL_Status eCLD_AlarmsResetAlarmLog(
tsZCL_EndPointDefinition *psEndPointDefinition,
tsZCL_ClusterInstance *psClusterInstance);
Description#
This function can be called on the Alarms cluster server to clear all entries of the local Alarms table. The function may be called as the result of user input.
Parameters#
psEndPointDefinition: Pointer to the ZCL endpoint definition structure for the application (see Section 6.1.1)
psClusterInstance: Pointer to structure containing information about the Alarms cluster instance (see Section 6.1.16)
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_AlarmsAddAlarmToLog#
teZCL_Status eCLD_AlarmsAddAlarmToLog(
tsZCL_EndPointDefinition *psEndPointDefinition,
tsZCL_ClusterInstance *psClusterInstance,
uint8 u8AlarmCode,
uint16 u16ClusterId);
Description#
This function can be called on the Alarms cluster server to add a new entry to the local Alarms table. The function should be called by the server application when an alarm condition has occurred. The alarm and the cluster which generated it must be specified. A timestamp (UTC) for the alarm is automatically inserted into the entry.
Parameters#
psEndPointDefinition: Pointer to the ZCL endpoint definition structure for the application (see Section 6.1.1)
psClusterInstance: Pointer to structure containing information about the Alarms cluster instance (see Section 6.1.16)
u8AlarmCode: Code that identifies the type of alarm to be added
u16ClusterId: Cluster ID of the cluster which generated the alarm
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_AlarmsGetAlarmFromLog#
teZCL_Status eCLD_AlarmsGetAlarmFromLog(
tsZCL_EndPointDefinition *psEndPointDefinition,
tsZCL_ClusterInstance *psClusterInstance,
uint8 *pu8AlarmCode,
uint16 *pu16ClusterId,
uint32 *pu32TimeStamp);
Description#
This function can be called on the Alarms cluster server to obtain an entry from the local Alarms table. Information on the logged alarm with the earliest timestamp in the device’s Alarms table is returned - pointers to memory locations to receive the retrieved alarm data must be provided. As a result of this command, the retrieved entry is also deleted from the table.
Parameters#
psEndPointDefinition: Pointer to the ZCL endpoint definition structure for the application (see Section 6.1.1)
psClusterInstance: Pointer to structure containing information about the Alarms cluster instance (see Section 6.1.16)
pu8AlarmCode: Pointer to location to receive the alarm code which identifies the retrieved alarm type
pu16ClusterId: Pointer to location to receive the Cluster ID of the cluster which generated the alarm
pu32TimeStamp: Pointer to location to receive timestamp (UTC) of the retrieved alarm (a value of 0XFFFFFFFF indicates that no timestamp is available for the alarm)
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_AlarmsSignalAlarm#
teZCL_Status eCLD_AlarmsSignalAlarm(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
uint8 u8AlarmCode,
uint16 u16ClusterId);
Description#
This function can be called on the Alarms cluster server to send an Alarm notification to a cluster client and add a log entry to the local Alarms table on the server. The function should be called by the server application when an alarm condition has occurred. The alarm and the cluster which generated it must be specified.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent
psDestinationAddress: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
u8AlarmCode: Code which identifies the type of alarm that has occurred
u16ClusterId: Cluster ID of the cluster which generated the alarm
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
Parent topic:Alarms Cluster