MCUXpresso SDK Documentation

eCLD_AlarmsResetAlarmLog

eCLD_AlarmsResetAlarmLog#

teZCL_Status eCLD_AlarmsResetAlarmLog(
    tsZCL_EndPointDefinition *psEndPointDefinition,
    tsZCL_ClusterInstance *psClusterInstance);

Description#

This function can be called on the Alarms cluster server to clear all entries of the local Alarms table. The function may be called as the result of user input.

Parameters#

  • psEndPointDefinition: Pointer to the ZCL endpoint definition structure for the application (see Section 6.1.1)

  • psClusterInstance: Pointer to structure containing information about the Alarms cluster instance (see Section 6.1.16)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions