MCUXpresso SDK Documentation

eCLD_AlarmsCommandResetAlarmLogCommandSend

eCLD_AlarmsCommandResetAlarmLogCommandSend#

teZCL_Status eCLD_AlarmsCommandResetAlarmLogCommandSend(
  uint8 u8SourceEndPointId,
  uint8 u8DestinationEndPointId,
  tsZCL_Address *psDestinationAddress,
  uint8 *pu8TransactionSequenceNumber);

Description#

This function can be called on an Alarms cluster client to send a Reset Alarm Log command to a cluster server. This command requests that the Alarms table on the server is cleared of all entries. The function may be called as the result of user input.

On receiving the command, an E_CLD_ALARMS_CMD_RESET_ALARM_LOG event is generated on the cluster server to notify the application but the ZCL automatically clears the Alarms table.

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent

  • psDestinationAddress: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions