ZPS_eAplZdpMgmtPermitJoiningRequest
ZPS_teStatus ZPS_eAplZdpMgmtPermitJoiningRequest(
PDUM_thAPduInstance hAPduInst,
ZPS_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS_tsAplZdpMgmtPermitJoiningReq
*psZdpMgmtPermitJoiningReq);
Description
This function requests a remote node to enable or disable joining for a specified amount of time. The destination node of this request must be a Router or the Co- ordinator. The request can be unicast to a particular node or broadcast to all routing nodes (for which the destination address must be set to the 16-bit network address 0xFFFC).
Note: This function is provided in the ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED.
The duration of the enable or disable joining state must be specified in the request. The request is represented by the structure below (further detailed in Section8.2.2.39).
typedef struct {
uint8 u8PermitDuration; bool_t bTcSignificance;
} ZPS_tsAplZdpMgmtPermitJoiningReq;
If the request was unicast, the remote node replies with a Mgmt_Permit_Joining_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpMgmtPermitJoiningRsp(detailed in Section 8.2.3.39).
Parent topic:ZPS_eAplZdpMgmtPermitJoiningRequest
Parameters
hAPduInst Handle of APDU instance in which request is sent.
uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)
bExtAddr Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
* pu8SeqNumber Pointer to sequence number of request
* psZdpMgmtPermitJoiningReqPointer to request (see above)
Parent topic:ZPS_eAplZdpMgmtPermitJoiningRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpMgmtLeaveRequest
Parent topic:ZPS_eAplZdpMgmtDirectJoinRequest
Parent topic:ZPS_eAplZdpMgmtPermitJoiningRequest
Parent topic:ZPS_eAplZdpMgmtCacheRequest
Parent topic:Network Management Services functions