ZPS_tsAplZdpMgmtPermitJoiningReq
This structure is used by the function ZPS_eAplZdpMgmtPermitJoiningRequest(). It requests a remote node (Router or Coordinator) to enable or disable joining for a specified amount of time.
The ZPS_tsAplZdpMgmtPermitJoiningReqstructure is detailed below.
typedef struct {
uint8 u8PermitDuration; bool_t bTcSignificance;
} ZPS_tsAplZdpMgmtPermitJoiningReq;
where:
u8PermitDurationis the time period, in seconds, during which joining will be allowed (0x00 means that joining is enabled or disabled with no time limit)bTcSignificancedetermines whether the remote device is a ‘Trust Centre’:TRUE: A Trust Centre
FALSE: Not a Trust Centre
Parent topic:ZDP Request structures