ZPS_eAplZdpMgmtCacheRequest#
ZPS_teStatus ZPS_eAplZdpMgmtCacheRequest(
PDUM_thAPduInstance hAPduInst,
ZPS_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS_tsAplZdpMgmtCacheReq *psZdpMgmtCacheReq);
Description#
This function requests a remote node to provide a list of the End Devices registered in its primary discovery cache. Therefore, the destination node must contain a primary discovery cache.
Note: This function is provided in the ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED.
The request is represented by the structure below (further detailed in Section9.2.2.40).
typedef struct {
uint8 u8StartIndex;
} ZPS_tsAplZdpMgmtCacheReq;
The remote node replies with a Mgmt_Cache_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpMgmtCacheRsp(detailed in Section 9.2.3.40).
Parent topic:ZPS_eAplZdpMgmtCacheRequest
Parameters#
hAPduInst Handle of APDU in which request is sent.
uDstAddr Address of destination node of request
(can be 16- or 64-bit, as specified by bExtAddr)
bExtAddr Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
* pu8SeqNumber Pointer to sequence number of request
* psZdpMgmtCacheReq Pointer to request (see above)
Parent topic:ZPS_eAplZdpMgmtCacheRequest
Returns#
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpMgmtLeaveRequest
Parent topic:ZPS_eAplZdpMgmtDirectJoinRequest
Parent topic:ZPS_eAplZdpMgmtPermitJoiningRequest
Parent topic:ZPS_eAplZdpMgmtCacheRequest
Parent topic:Network Management Services functions