Hardware requirements#
Mini/micro USB cable
MIMXRT1060-EVKC board
Personal Computer
Board settings#
MCUBoot layout#
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x60000000 |
0x6003FFFF |
256kB |
Primary slot |
0x60040000 |
0x6023FFFF |
2048kB |
Secondary slot |
0x60440000 |
0x6083FFFF |
2048kB |
MCUBoot header size is set to 1024 bytes
Signing algorithm is ECDSA-P256
Write alignment is 4 bytes
MCUBoot is configured to use its DIRECT_XIP image handling strategy
Flash remapping HW feature is used for zero-overhead image swapping
Image signing example#
imgtool sign --key sign-ecdsa-p256-priv.pem
--align 4
--version 1.1
--slot-size 0x200000
--header-size 0x400
--pad-header
ota_mcuboot_basic.bin
ota_mcuboot_basic.SIGNED.bin
Note that for the first image flashed manually together with the bootloader additional imgtool options “–pad” and “–confirm” must be used. Otherwise the bootloader would reject the image for missing data in the trailer area.
Custom configuration - Encrypted XIP#
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x60000000 |
0x6003FFFF |
256kB |
Primary slot |
0x60040000 |
0x6023FFFF |
2048kB |
Secondary slot |
0x60240000 |
0x6043FFFF |
2048kB |
Encryption metadata |
0x60440000 |
0x60440FFF |
4kB |
This custom build generates a project with predefined configuration to utilize Encrypted XIP mode. For more information please see Encrypted XIP and MCUboot.
MCUBoot header size is set to 1024 bytes
Signing algorithm is ECDSA-P256
Write alignment is 4 bytes
MCUBoot is configured for
Encrypted XIP modeusing modifiedMCUBOOT_OVERWRITE_ONLYimage update strategyMCUboot uses ECDH-P256 to secure AES key for image encryption
Primary slot is encrypted by BEE module to utilize encrypted XIP
Image signing example:
imgtool sign --key sign-ecdsa-p256-priv.pem
--align 4
--version 1.1
--slot-size 0x200000
--header-size 0x400
--max-sectors 59
--pad-header
-E enc-ec256-pub.pem
ota_mcuboot_basic.bin
ota_mcuboot_basic.SIGNED.bin
Project building example:
The project is built using west tool. For more information please see MCUXpresso SDK documentation.
Bootloader:
west build -p always examples/ota_examples/mcuboot_opensource --toolchain iar --config flexspi_nor_debug -b evkcmimxrt1060 -t guiproject -DCONF_FILE="examples/ota_examples/_custom_cfg/rt10xx/mcuboot_opensource.conf" -d builds/mcuboot
OTA application:
west build -p always examples/ota_examples/ota_mcuboot_basic --toolchain iar --config flexspi_nor_debug -b evkcmimxrt1060 -t guiproject -DCONF_FILE="examples/ota_examples/_custom_cfg/rt10xx/ota_mcuboot_basic.conf" -d builds/ota_mcuboot_basic