Encrypted XIP and MCUboot#
1. Introduction#
To provide confidentiality of image data while in transport to the device or while residing on an non-secure storage such as external flash memory, MCUboot has support for encrypting/decrypting images on-the-fly while upgrading. MCUboot architecture expects that XIP is done from a secure memory so encrypted image is decrypted to a secure location such as internal Flash or RAM, however, size of an internal RAM is limited and there are devices with interfaces to only external flash memory.
Some NXP devices support encrypted XIP on an internal or external Flash device utilizing on-the-fly decryption modules (BEE, OTFAD, IPED, NPX…). Is possible use these decryption engines with a second stage bootloader as the MCUboot.
This document describes an extension of MCUboot functionality to support encrypted XIP on NXP devices and its enablement in OTA examples in MCUXpresso SDK.
2. MCUboot encrypted image#
In the extension, the image encrypted by MCUboot is used as a secure capsule for transport and staging in the non-XIP area of a device. For more information please see MCUboot Encrypted images documentation.
In summary, an image payload is encrypted using AES-CTR cipher by image tool (see imgtool). The AES key is randomized per OTA image and padded to image as an encrypted TLV section. The encrypted AES key can be decrypted using private key in selected key encryption scheme (RSA-OAEP, AES-KW, ECIES-P256 or ECIES-X25519).
Following image shows keys management of MCUboot encrypted image.

As shown in the image, a user must securely embed the encryption private key into the device. For simplicity, the OTA examples in SDK use private keys embedded as a C array in MCUboot code (see middleware\mcuboot_opensource\boot\nxp_mcux_sdk\keys.c). Users are advised to implement secure provisioning and loading of the private key in the device, for example by encrypting the MCUboot application (including the array) using the encrypted XIP feature of the device, or by staging the private key in trusted sources like OTP or TPM (supported since MCUboot 2.2.0).
3. Encrypted XIP extension for MCUboot#
The extension combines usage of platform specific encrypted XIP feature and funcionality of MCUboot encrypted images created by imgtool.
Following image shows simplified OTA update flow of device fleet using encrypted XIP extension.

The device fleet shares a common MCUboot private key used for decryption of encrypted OTA images residing in staging areas. The MCUboot AES key and hardware encryption module are then used for image re-encryption to the execution area. The hardware key is provisioned by NXP or the user and is typically unique per device instance to prevent image cloning
3.1 Configuration structures#
In summary, every NXP encryption module utilizing the encrypted XIP feature uses a scheme where on-the-fly decryption is configured by ROM. After device reset, the ROM investigates specific configuration structures typically expected at a particular flash offset in the header of the bootable image, which is MCUboot in our case. If configuration structures consisting of encrypted keys and IVs are valid, then the ROM configures the encryption module for encrypted XIP.
In the case of an OTA update, it is expected that for security reasons we have to update the key or IV of the encrypted execution region, so these configuration blocks also have to be re-generated for each OTA update. Unfortunately, this creates a risk during the update of these configuration blocks, as there is a period of time where a power loss could corrupt the update and result in a bricked device.
Note: The risk is related only to use cases using a custom second-stage bootloader. OTA solutions using only a ROM bootloader typically utilize a dual image feature which safely handles this issue, as the ROM can safely revert to the last functional configuration.
The risk is resolved by moving configuration blocks out of the header of the second stage bootloader to a particular flash area and letting the bootloader configure the encryption module manually by inspecting these configuration blocks.

There is always one static configuration for MCUboot used by ROM for encrypted XIP initialization during startup, and one or two dynamic configurations for application slots which are regenerated during an OTA update. These dynamic configuration blocks are manually handled by MCUboot or an OTA process to provide more flexibility and robustness to the update process.
In the case of a layout utilizing flash remap, the encryption of the MCUboot partition is optional. This is because there is no need for a private key, unlike in the overwrite-only layout, where slot 1 is offline encrypted by the MCUboot encryption mechanism.
Note: The following text focuses on overwrite-only mode as it is much simpler and universally implementable on all devices. Flash remap layout will be covered in separate application notes in future SDK releases.
The encrypted XIP extension uses a reserved area called encryption metadata which is used for storage of configuration blocks. The following image shows the general structure of encryption metadata.

The metadata sector consists of platform-specific configuration blocks and a common confirmation block. The slot number is a pointer to the slot containing the selected image extracted from the MCUboot response object. The hash acts as a confirmation of the integrity of configuration blocks and content in the execution slot.
It’s recommended to have both blocks in a common flash sector so they are separated by flash page granularity and deleted simultaneously during OTA updates. Typically, in the example code, the configuration block is placed at the beginning of the sector and the confirmation block is placed at the end of the sector.
During an OTA update, the extension generates a new configuration block with IV, writes it at a particular flash offset, and reconfigures the encryption unit for the execution area. If the update and verification of the execution area are successful, the configuration block is then hashed and confirmed by writing the confirmation block.
3.2 Partition layout#
The extension utilizes a partition layout with one execution slot for encrypted XIP and one slot for staging an OTA image.
Extension mode |
required flash size |
revert (self-test) support |
|---|---|---|
Modified overwrite-only |
SBL + 2 x slot size + metadata sector |
no |
Following image shows flash memory layout using MCUboot bootloader in MCUBOOT_OVERWRITE_ONLY mode and the encrypted XIP extension.

Secondary slots act as a staging area for encrypted OTA image by MCUboot. The execution slot is used as an execution area of the encrypted image using platform on-the-fly decryption.
Note: the placement of metadata in the flash memory is up to user.
3.3 Flow of modified overwrite only mode#
Following image shows simplified flow of MCUboot overwrite-only mode extended with encrypted XIP extension.

Before jumping to the booting process, the on-the-fly decryption is initialized so MCUboot is able to read and validate content in the primary slot. The re-encryption process is implemented in customized MCUboot code and in MCUboot hooks (see flash_api.c and bootutil_hooks.c).
4. NXP encryption engines#
4.1 BEE (Bus Encryption Engine)#
This peripheral is specific for RT10xx (except RT1010) and supports up to two separate regions using two separate AES keys. In the examples, BEE region 1 is used for encrypting the execution slot and BEE region 0 is reserved for a bootloader.
BEE configuration blocks are organized as EPRDB (Encrypted Protection Region Descriptor Block), where the EPRDB is encrypted using AES-CBC mode with AES key and IV located in KIB (Key Info Block). The KIB is encrypted as EKIB (Encrypted KIB) using a key provisioned by the user. Each BEE region has its PRDB/KIB pair.
The EKIB is decrypted by a key based on selection in BEE_KEYn_SEL fuse:
Software key
default value in
BEE_KEYn_SELevaluating BEE without fusing the device
SW-GP2
fused by user and typically used for offline encryption
limited funcionality due hardware bugs, see errata
not supported in the examples
OTPMK
provisioned by NXP in factory
unique per device instance - prevents image cloning
recommended
Following image shows complete metadata structure used for devices with BEE.

Firmware in execution slot is de/encrypted using AES-CTR combining nonce extracted from PRDB and this device key. The extension automatically detects device key by evaluating BEE_KEYn_SEL fuse.
The whole BEE initialization and encryption metadata handling is resolved in module encrypted_xip_platform_bee.c.
Additional information can be found in Security Reference Manual of target device and in application notes AN12800, AN12852 and AN12901.
4.2 OTFAD (On-the-Fly AES Decryption Module)#
To be implemented…
4.3 IPED (Inline Prince Encryption/Decryption for off-chip flash)#
IPED is encryption unit for external flash specific for NXP RW61x, RT700 and MCXN MCUs.
Note: The extension currently supports only IPED module based on GCM algorithm in RW61x devices.
Following image shows configuration of metadata structure used for devices with IPED.

There are several points when using IPED especially in GCM mode
Consumption of physical memory when GCM algorithm is used
range of IPED region is defined in terms of logical address but the physical memory consumption is 1.25 times the logical memory consumption
OTA process must ensure that installed OTA image doesn’t overlap size of IPED region, for example by adjusting the text size in linker file and doing checks of re-encrypted image size
Flash operations have to satisfy boundaries of the flash page/sector size and encryption unit size
see “Constraints on IPED regions” chapter in reference manual
The whole IPED initialization and encryption metadata handling is resolved in module encrypted_xip_platform_iped.c.
Additional information for IPED in RW61x can be found in its reference manual.
4.4 NPX (PRINCE encryption/decryption for on-chip flash)#
See separate documentation for NPX.
5. OTA examples instructions#
Start preferentially with an empty board, erasing original content if needed.
5.1 Generate ECIES-P256 key pairs for encrypted image containers (optional)#
Note: This part can be skipped as OTA examples in SDK uses pre-generated key pairs.
Generate private key using imgtool:
imgtool keygen -k enc-ec256-priv.pem -t rsa-2048Adjust the content of the
middleware\mcuboot_opensource\boot\nxp_mcux_sdk\keys\enc-ec256-priv.pemaccordingly.
Extract private key to a C array:
imgtool getpriv --minimal -k enc-ec256-priv.pemAdjust the content of the
middleware\mcuboot_opensource\boot\nxp_mcux_sdk\keys\enc-ec256-priv-minimal.caccordingly.
Derive public key key:
imgtool getpub -k enc-ec256-pub.pem -e pemAdjust the content of themiddleware\mcuboot_opensource\boot\nxp_mcux_sdk\keys\enc-ec256-pub.pemaccordingly.
5.2 Enable encrypted XIP support and build projects#
There are three ways how to enable Encrypted XIP mode:
Manually modify content of
sblconfig.hEnable
CONFIG_ENCRYPT_XIP_EXT_ENABLEDisable
CONFIG_MCUBOOT_FLASH_REMAP_ENABLEandCONFIG_BOOT_CUSTOM_DEVICE_SETUP
Manually customize Kconfig configuration and generate the project - see Kconfig and customization of OTA examples
Use pre-defined customized builds - see particular chapter in your board readme (see Supported boards)
Then build and load the mcuboot_opensource application.
5.3 Sign and encrypt image#
To sign and encrypt an application binary, imgtool must be provided with the respective key pairs and a set of parameters as in the following examples.
imgtool sign --key sign-ecdsa-p256-priv.pem
--align 4
--header-size 0x400
--pad-header
--slot-size 0x200000
--max-sectors 800
--version "1.1"
-E enc-ec256-pub.pem
app_binary.bin
app_binary_SIGNED_ENCRYPTED_OTA.bin
The values of parameters can be obtained from a readme file of target board. Example: boards\BOARD\ota_examples\mcuboot_opensource\example_board_readme.md
5.4 Evaluate encrypted XIP example#
There are two methods how to run device for first time when application uses encrypted XIP.
5.4.1 Load encrypted image container to flash memory#
See flash_partitioning.h for your board.
/* Encrypted XIP extension: modified overwrite-only mode */
#define BOOT_FLASH_ACT_APP 0x60040000 -- active (execution) slot address
#define BOOT_FLASH_CAND_APP 0x60240000 -- candidate slot address
#define BOOT_FLASH_ENC_META 0x60440000 -- encryption metada address
Encrypted image by MCUboot has to be loaded always to candidate slot address defined as BOOT_FLASH_CAND_APP.
To load image the pyocd, blhost or MCUXpresso Secure Provisioning Tool can be used.
5.4.2 Run unsigned unencrypted OTA application (debug session)#
An unsigned unencrypted application can be loaded and run from execution area using a debug session as usual.
5.5 Running encrypted image#
These are expected outputs when an OTA image is detected and then re-encrypted
hello sbl.
Bootloader Version 2.1.0
On-the-fly decryption initialization completed
Image index: 0, Swap type: test
Image 0 upgrade secondary slot -> primary slot
Erasing the primary slot
On-the-fly decryption initialization completed
Image 0 copying the secondary slot to the primary slot: 0x9734 bytes
writing magic; fa_id=0 off=0x1ffff0 (0x23fff0)
erasing secondary header
erasing secondary trailer
Bootloader chainload address offset: 0x40000
Reset_Handler address offset: 0x40400
Jumping to the image
*************************************
* Basic MCUBoot application example *
*************************************
Built Feb 13 2025 16:06:06
$
6. Supported boards#
BEE:
IPED:
NPX: