MCUXpresso SDK Documentation

eCLD_ZllCommissionCreateCommission

eCLD_ZllCommissionCreateCommission#

teZCL_Status eCLD_ZllCommissionCreateCommission(
    tsZCL_ClusterInstance *psClusterInstance,
    bool_t bIsServer,
    tsZCL_ClusterDefinition *psClusterDefinition,
    void *pvSharedStructPtr,
    tsZCL_AttributeStatus *psAttributeStatus,
    tsCLD_ZllCommissionCustomDataStructure
*psCustomDataStructure);

Description#

This function creates a Touchlink Commissioning cluster instance for Touchlink on the endpoint of the calling application. The type of cluster instance (server or client) to be created must be specified.

In practice, this function does not need to be called explicitly by the application, as the function eZLL_RegisterCommissionEndPoint() calls this function to create the cluster instance.

Parameters#

  • psClusterInstance        Pointer to cluster instance structure on local endpoint

  • bIsServer        Type of cluster instance (server or client) to be created:

  • TRUE - server

  • FALSE - client

  • psClusterDefinition        Pointer to cluster definition structure containing information about the cluster

  • pvSharedStructPtr        Pointer to structure containing the shared storage for the cluster

  • psAttributeStatus        Pointer to a structure containing the storage for each attribute’s status

  • psCustomDataStructure        Pointer to custom data to be provided to the cluster (see Section 44.8.3)

Returns#

  • E_ZCL_SUCCESS

Parent topic:Touchlink functions