tsCLD_ZllCommissionCustomDataStructure
This structure is used to hold the data for a Touchlink command received by a node.
typedef struct
{
tsZCL_ReceiveEventAddressInterPan sRxInterPanAddr;
tsZCL_CallBackEvent sCustomCallBackEvent;
tsCLD_ZllCommissionCallBackMessage sCallBackMessage;
} tsCLD_ZllCommissionCustomDataStructure;
where:
RxInterPanAddris a ZCL structure containing the Inter-PAN addresses of the source and destination nodes of the command.sCustomCallBackEventis the ZCL event structure for the command.sCallBackMessageis a structure containing the command ID and payload (see Section 44.8.4).
Parent topic:Structures