eCLD_ScenesCommandCopySceneSceneRequestSend#
teZCL_Status eCLD_ScenesCommandCopySceneSceneRequestSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_ScenesCopySceneRequestPayload *psPayload);
Description#
This function sends a Copy Scene command to a remote device, requesting that the scene settings from one scene ID/group ID combination are copied to another scene ID/group ID combination on the target endpoint. The relevant source and destination scene ID/group ID combinations are specified in the command payload.
Note that:
If the destination scene ID/group ID exists on the target endpoint, the existing scene is overwritten with the new settings.
The message payload contains a ‘copy all scenes’ bit. If the bit is set to ‘1’, it instructs the destination server to copy all scenes in the specified source group to scenes with the same scene IDs in the destination group. In this case, the source and destination scene IDs in the payload are ignored.
The device receiving this message generates a callback event on the endpoint on which the Scenes cluster was registered and, if the original request is unicast, generates a Copy Scene response (see Section 13.7.3).
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address type eZCL_AMBOUND.
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2).
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions