MCUXpresso SDK Documentation

eCLD_ScenesCommandAddSceneRequestSend

eCLD_ScenesCommandAddSceneRequestSend#

teZCL_Status eCLD_ScenesCommandAddSceneRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesAddSceneRequestPayload *psPayload);

Description#

This function sends an Add Scene command to a remote device in order to add a scene on the specified endpoint - that is, to add an entry to the Scene table on the endpoint. The scene ID is specified in the payload of the message, along with a duration for the scene among other values (see Section 13.7.2). The scene may also be associated with a particular group.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster is registered and, if possible, add the scene to its Scene table before sending an Add Scene response indicating success or failure (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

    • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions