eCLD_OnOffCommandOnWithTimedOffSend
teZCL_Status eCLD_OnOffCommandOnWithTimedOffSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_OnOff_OnWithTimedOffRequestPayload
*psPayload);
Description
This function sends a custom ‘On With Timed Off’ command instructing the target lighting device to switch on one or more lights for a timed period and then switch them off. In addition, a waiting time can be implemented after switch-off, during which the lights cannot be switched on again.
The following functionality must be specified in the command payload:
Time for which the lights must remain on.
Waiting time during which switched-off lights cannot be switched on again.
Whether this command can be accepted at any time (outside the waiting time) or only when a light is on.
For the payload details, refer to “On With Timed Off Request Payload”.
The device receiving this message generates a callback event on the endpoint on which the On/Off cluster was registered.
If used, the ‘On With Timed Off’ command must be enabled in the compile-time options on both the client and server, as described in Section 14.10.
Parameters
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types
eZCL_AMBOUNDandeZCL_AMGROUP.psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
psPayload: Pointer to a structure containing the payload for this message (see Section 14.8.2).
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions