Compile-time options
To enable the On/Off cluster in the code to be built, it is necessary to add the following to the zcl_options.h file:
#define CLD_ONOFFIn addition, to include the software for a cluster client or server or both, it is necessary to add one or both of the following to the same file:
#define ONOFF_CLIENT #define ONOFF_SERVER
The On/Off cluster contains macros that may be optionally specified at compile time by adding some or all of the following lines to the zcl_options.h file.
Optional Attributes
To enable the optional On Configurable Duration attribute, add this line:
#define CLD_ONOFF_ATTR_ID_ON_CONFIGURABLE_DURATIONTo enable the optional Duration Unit of Measure attribute, add this line:
#define CLD_ONOFF_ATTR_ID_DURATION_UNIT_OF_MEASUREMENTTo enable the optional Maximum Duration attribute, add this line:
#define CLD_ONOFF_ATTR_ID_MAX_DURATIONTo enable the optional Global Scene Control attribute, add this line:
#define CLD_ONOFF_ATTR_GLOBAL_SCENE_CONTROLTo enable the optional On Time attribute, add this line:
#define CLD_ONOFF_ATTR_ON_TIMETo enable the optional Off Wait Time attribute, add this line:
#define CLD_ONOFF_ATTR_OFF_WAIT_TIMETo enable the optional Start-up On/Off attribute, add this line:
#define CLD_ONOFF_ATTR_STARTUP_ONOFFTo enable the optional Attribute Reporting Status attribute, add this line:
#define CLD_ONOFF_ATTR_ID_ATTRIBUTE_REPORTING_STATUS
Optional Commands
Add this line to enable processing of the On With Recall Global Scene command on the server:
#define CLD_ONOFF_CMD_ON_WITH_RECALL_GLOBAL_SCENEAdd this line to enable the optional On With Timed Off command on the client and server:
#define CLD_ONOFF_CMD_ON_WITH_TIMED_OFFAdd this line to enable the optional Off With Effect command on the client and server:
#define CLD_ONOFF_CMD_OFF_WITH_EFFECT
Cluster Revision
To define the value (n) of the Cluster Revision attribute, add this line:
#define CLD_ONOFF_CLUSTER_REVISION <n>
The default value is 1, which corresponds to the revision of the cluster in the ZCL r6 specification (see Section 2.4).
Parent topic:On/Off Cluster