BDB_tuBdbEventData#
The following structure is a union containing the data for a ZigBee Base Device event.
typedef union
{
BDB_tsZpsAfEvent sZpsAfEvent;
BDB_tsFindAndBindEvent *psFindAndBindEvent;
}BDB_tuBdbEventData
where:
sZpsAfEventis a structure containing the data for a stack event, indicated by the event type BDB_EVENT_ZPSAF - for a description of this structure, refer to Section 2.7.3.psFindAndBindEventis a pointer to a structure containing the data for a ‘Finding and Binding’ event (see Section 2.9) - for a description of this structure, refer to Section 2.7.4.
Parent topic:Structures