MCUXpresso SDK Documentation

BDB_tsZpsAfEvent

BDB_tsZpsAfEvent#

The following structure contains the data for a ZigBee stack event (see the BDB_EVENT_ZPSAF event in Section 2.9).

typedef struct
{
    uint8 u8EndPoint;
    ZPS_tsAfEvent sStackEvent;
}BDB_tsZpsAfEvent;

where:

  • u8EndPoint is the number of the endpoint on which the event occurred.

  • sStackEvent is a ZPS structure containing the stack event type and data - this structure is detailed in the ZigBee 3.0 Stack User Guide (JNUG3130).

Parent topic:Structures